Skip to search Skip to main content Skip to navigation

Your feedback matters, take a quick surveyWebsite feedback

We noticed you are from . Visit your local site for regional offers and live support.
Technical Learning Installation Obstacles: Invasive In-Pipe Immersion Sensors

Installation Obstacles: Invasive In-Pipe Immersion Sensors When it comes to process piping systems, temperature of in-pipe media is often a necessary measurement – and one that needs to be monitored accurately. Traditionally, in-pipe immersion sensors are used. However, invasive in-pipe immersion sensors are often not ideal for use within process piping systems. Here are 3 considerations to take before installing immersion sensors in process piping systems.

Read More
Technical Learning How to Monitor Asphalt Temperature with IIoT Devices

How to Monitor Asphalt Temperature with IIoT Devices The temperature of hot mixed asphalt is a critical component to the compaction and longevity of poured concrete.

Read More
Technical Learning How to Connect Your Modbus Devices to the Omega Link Gateway

How to Connect Your Modbus Devices to the Omega Link Gateway Industrial setups look to reap the benefits of the Industrial Internet of Things (IIoT) by establishing a connected environment.

Read More
Technical Learning What is Edge Computing?

What is Edge Computing? The concept of edge computing has been around for several years, stemming from the days of on-premise Computer Instrumentation or Human Machine Interface (HMI) computers.

Read More
Application

How to Bend Guitar Sides with a Silicone Heater There are several ways to bend guitar sides, including the traditional method of using a hot pipe. However, a faster and more cost-efficient method, which has become common, involves using flexible silicone heaters with a flexible thermocouple and controller.

Read More
Technical Learning 4-20mA Input

4-20mA Input It is extremely simple and inexpensive to measure 4-20ma signal with a device that will measure only Voltage inputs.

Read More
Technical Learning Digital Signal Transmission

Digital Signal Transmission In contrast to analog transducers that sense continuous variables such as pressure and temperature, many transducers provide an output that is one of two states: high or low, open or closed.

Read More
Technical Learning What are silicone heaters used for?

What are silicone heaters used for? Silicone rubber heaters have a wide range of industrial, commercial, and military applications. These heaters are resistant to radiation, moisture, compression set, weathering, vacuum, fungus, oils, solvents, and chemical attack.

Read More
Technical Learning Ship Engine Room Technology Upgrade

Ship Engine Room Technology Upgrade A globally operating shipping and logistics company recently decided to refurbish a number of ships with newer technology.

Read More
Technical Learning Danish CHP Station

Danish CHP Station The members of a maintenance team at a Danish power station were fed up getting error messages and false system alarms from one of the boiler’s temperature surveillance systems.

Read More
Technical Learning What is a Vortex Flow Meter?

What is a Vortex Flow Meter? A vortex flow meter is a flow measurement device best suited for flow measurements where the introduction of moving parts presents problems.

Read More
Case Study Connecting Relays to a Digital Output Board and Noise Considerations

Connecting Relays to a Digital Output Board and Noise Considerations Mechanical relays are very noisy (electrically) and they can cause problems when connecting them to a PC digital I/O card, ranging from spikes on your analog measurements to computer lockups!

Read More
Product Info How to choose a Thermocouple

How to choose a Thermocouple There are different types of thermocouples and their applications may vary. An exposed thermocouple will work best when high response times are required, but an ungrounded thermocouple is better in corrosive environments

Read More
Product Info What Are the Differences Between 2-Wire, 3-Wire, and 4-Wire RTD Configurations?

What Are the Differences Between 2-Wire, 3-Wire, and 4-Wire RTD Configurations? A Resistance Temperature Detector (RTD) measures temperature using a resistor with a resistance value that changes as its temperature increases or decreases.

Read More
Technical Learning What is a Voltage Divider?

What is a Voltage Divider? In order to measure a signal which varies over a range greater than the input range of an analog or digital input of a measuring device, a voltage divider can drop the voltage of the input signal to the level the analog or digital input can measure.

Read More
Technical Learning Common Problems with Data Acquisition Devices

Common Problems with Data Acquisition Devices Traditional printer drivers are very benign; they are only active, and use the printer port when you tell an application to print.

Read More
Technical Learning Infrared Quick Help

Infrared Quick Help When to Use Infrared Temperature Measurement

Read More
Product Info Temperature Control Using PID

Temperature Control Using PID Almost every process control application would benefit from PID control.

Read More
Technical Learning Mechanical Flow meters

Mechanical Flow meters Discussed in this chapter are various types of mechanical flow meters that measure flow using an arrangement of moving parts,

Read More
Technical Learning Types of Flow Meters for Different Applications

Types of Flow Meters for Different Applications Measuring the flow of liquids is a critical need in many industrial plants.

Read More
Technical Learning Plug-in Cards

Plug-in Cards Although the microprocessor and digital network technologies have fundamentally reinvented the ways in which today's data acquisition systems handle data

Read More
Technical Learning Differential Signal Vs Single-Ended Inputs

Differential Signal Vs Single-Ended Inputs One of the most common questions asked is the difference between single-ended and differential signals inputs, and what applications they should be considered in.

Read More
Technical Learning The RS-232 protocol

The RS-232 protocol Information being transferred between data processing equipment and peripherals is in the form of digital data which is transmitted in either a serial or parallel mode.

Read More
Technical Learning Specialty Level Switches

Specialty Level Switches Thermal, vibrating, and optical level switches are specialty devices developed to solve specific level detection problems.

Read More
Technical Learning Reactive Maintenance vs. Proactive Maintenance: You’re Paying 2-5X More for Maintenance

Reactive Maintenance vs. Proactive Maintenance: You’re Paying 2-5X More for Maintenance Proactive maintenance, reactive maintenance, and the many benefits of switching to proactive maintenance.

Read More
Technical Learning Industry 4.0 — The Next Industrial Revolution

Industry 4.0 — The Next Industrial Revolution Imagine a manufacturing facility where everything goes as planned.

Read More
Case Study How Rutgers Food Innovation Center Used Automation to Boost Food Quality and Save Time

How Rutgers Food Innovation Center Used Automation to Boost Food Quality and Save Time We definitely don’t want to go back to the way we were doing it. It was too much work and didn’t pay off. –Steve Baughman, Senior Maintenance Mechanic for Rutgers Food Innovation Center

Read More
Technical Learning Improving Safety in Machine Control Systems with Limit Switches

Improving Safety in Machine Control Systems with Limit Switches Imagine a product being moved on a conveyor belt that somehow gets out of place.

Read More
Technical Learning 10 Applications Where You Need a Digital Panel Meter

10 Applications Where You Need a Digital Panel Meter Digital panel meters present numerical information that’s easy to read.

Read More
Technical Learning Infrared Temperature Measurement Theory and Application

Infrared Temperature Measurement Theory and Application Infrared thermometers for non-contact temperature measurement are highly developed sensors which have wide-spread application in...

Read More
Technical Learning Types of Load Cells

Types of Load Cells Various load cell types are preferred, relative to the needs of the laboratory or operational environment.

Read More
Product Info IC Sensors

IC Sensors An IC Temperature Sensor is a two terminal integrated circuit temperature transducer that produces an output current proportional to absolute temperature. The sensor package is small with a low thermal mass and a fast response time

Read More
Product Info Data Acquisition

Data Acquisition In the simplest form, a technician logging the temperature of an oven on a piece of paper is performing data acquisition.

Read More
Technical Learning How Bright is it? Shining a light on intensity measurement

How Bright is it? Shining a light on intensity measurement Human vision depends on light. Light reflects off surfaces into the eyes, passing through the cornea and pupil to form an image on the retina.

Read More
Product Info What is a Flexible Heater?

What is a Flexible Heater? A flexible heater is a device which can conform to the surface which requires heating.

Read More
Product Info Data Loggers

Data Loggers Technically speaking, a data logger is any device that can be used to store data.

Read More
Product Info Thermocouple Wire

Thermocouple Wire Wire that is used in a thermocouple from the point of sensing to the point of cold junction compensation (cjc end) where the signal is measured.

Read More
Product Info What are Electromagnetic Flow Meters?

What are Electromagnetic Flow Meters? A magnetic flow meter (mag flow meter) is a volumetric flow meter which does not have any moving parts and is ideal for wastewater applications or any dirty liquid which is conductive or water based.

Read More
Product Info Immersion Heater

Immersion Heater An immersion heater is a device which is installed in a tank or container to heat a liquid. The installation can be over-the-side, flanged or threaded.

Read More
en-US
en
Save Configuration