![An Introduction to 3-A Sensors for Sanitary Applications](https://assets.omega.com/resources/3a-sensors-sanitary-applications-uf.png)
An Introduction to 3-A Sensors for Sanitary Applications 3-A standards were developed in the 1920’s as way to qualify processes as being sanitary. The objective is to prevent contamination of products produced for human consumption or direct contact.
Tagged as:Technical Learning, Get Curious
Read More![](https://assets.omega.com/resources/ultrasonic-flow-meter-water-leak-us.png)
How to Locate a Water Leak Using an Ultrasonic Flow Meter When a single conduit line in a complex configuration of pipelines is compromised, it can be challenging to locate the precise point where the leak is occurring.
Tagged as:Application, Get Curious
Read More![](https://assets.omega.com/resources/flow-meter-paper-stock-us.jpg)
Flow of Paper Stock A customer in the paper industry wanted to measure flow of paper stock pulp on a 250mm SS line with an average flow of 120-150 l/s and a pulp temperature of 45°.
Tagged as:Application, Get Curious
Read More![](https://assets.omega.com/resources/flow-measurement-microbreweries-uf.jpg)
Sanitary Precision Flow Measurement for Microbreweries All microbreweries need the ability to measure the liquid flow of their product in a manner that is sanitary and meets FDA regulations.
Tagged as:Application, Get Curious
Read More![An Introduction to Flow Meters](https://assets.omega.com/resources/flowmeters-uf.jpg)
An Introduction to Flow Meters As the name implies a Flow meter is an instrument for monitoring, measuring, or recording the rate of flow, pressure, or discharge of liquids or gasses.
Tagged as:Product Info, Get Curious
Read More![What is a Mass Flow Meter?](https://assets.omega.com/resources/thermal-mass-flow-meters-uf.jpg)
What is a Mass Flow Meter? A thermal mass flow meter measures the flow rate of gas mass based on the convective heat transfer of a heated surface to the flowing fluid.
Tagged as:Technical Learning, Get Curious
Read More![What is a Coriolis Flow Meter and How Does it Work?](https://assets.omega.com/resources/what-is-a-coriolis-flow-meter-uf.jpg)
What is a Coriolis Flow Meter and How Does it Work? A Coriolis flow meter is a type of mass flow meter. It is designed differently and works differently than thermal or differential mass flow meters.
Tagged as:Technical Learning, Get Curious
Read More![What is a Vortex Flow Meter?](https://assets.omega.com/resources/vortex-flow-meter-uf.jpg)
What is a Vortex Flow Meter? A vortex flow meter is a flow measurement device best suited for flow measurements where the introduction of moving parts presents problems.
Tagged as:Technical Learning, Get Curious
Read More![Flow Meter Tutorial](https://assets.omega.com/resources/flow-meter-tutorial-uf.jpg)
Flow Meter Tutorial So you want to measure flow? The answer would seem to be to purchase a flowmeter.
Tagged as:Technical Learning, Get Curious
Read More![Technical Principles of Valves](https://assets.omega.com/resources/valves-technical-principles-uf.jpg)
Technical Principles of Valves Solenoid valves are used wherever fluid flow has to be controlled automatically. They are being used to an increasing degree in the most varied types of plants and equipment.
Tagged as:Technical Learning, Get Curious
Read More![Top 6 Methods to Measure or Monitor Fluid Levels](https://assets.omega.com/resources/best-method-to-measure-or-monitor-fluid-levels-uf.jpg)
Top 6 Methods to Measure or Monitor Fluid Levels Measuring and monitoring fluid levels accurately and precisely requires choosing the correct methodology for the target medium and vessel.
Tagged as:Technical Learning, Get Going
Read More![Mechanical Flow meters](https://assets.omega.com/resources/t9904-08-mech-uf.jpg)
Mechanical Flow meters Discussed in this chapter are various types of mechanical flow meters that measure flow using an arrangement of moving parts,
Tagged as:Technical Learning, Get Curious
Read More![Differential Pressure Flow meters](https://assets.omega.com/resources/differential-pressure-flow-meter-uf.jpg)
Differential Pressure Flow meters The calculation of fluid flow rate by reading the pressure loss across a pipe restriction is perhaps the most commonly used flow measurement technique in industrial applications
Tagged as:Technical Learning, Get Curious
Read More![RF/Capacitance Level Instrumentation](https://assets.omega.com/resources/t9904-13-rf-cap-uf.jpg)
RF/Capacitance Level Instrumentation Capacitance level detectors are also referred to as radio frequency (RF) or admittance level sensors. They operate in the low MHz radio frequency range, measuring admittance of an alternating current (ac) circuit that varies with level.
Tagged as:Technical Learning, Get Curious
Read More![Types of Flow Meters for Different Applications](https://assets.omega.com/resources/flow-meter-types-uf.jpg)
Types of Flow Meters for Different Applications Measuring the flow of liquids is a critical need in many industrial plants.
Tagged as:Technical Learning, Get Curious
Read More![What is a Variable Area Flow Meter?](https://assets.omega.com/resources/variable-area-flow-uf.jpg)
What is a Variable Area Flow Meter? Variable area flow meters are simple and versatile devices that operate at a relatively constant pressure drop and measure the flow of liquids, gases, and steam.
Tagged as:Technical Learning, Get Curious
Read More![An Introduction to Venturi Flow Meters, Flow Nozzles, and Segmental Wedge Elements](https://assets.omega.com/resources/venturi-meter-uf.jpg)
An Introduction to Venturi Flow Meters, Flow Nozzles, and Segmental Wedge Elements Venturi tubes are available in sizes up to 7 inches and can pass 25 to 50% more flow than an orifice with the same pressure drop
Tagged as:Technical Learning, Get Curious
Read More![What is an Orifice Plate Flow Meter?](https://assets.omega.com/resources/orifice-plate-flow-meter-uf.jpg)
What is an Orifice Plate Flow Meter? The orifice plate flow meter is commonly used in clean liquid, gas, and steam services. It is available for all pipe sizes but it is very cost-effective for measuring flows in larger ones (over 6 inches diameter).
Tagged as:Technical Learning, Get Curious
Read More![An Introduction to Pitot Tubes and Probes](https://assets.omega.com/resources/pitot-tube-uf.jpg)
An Introduction to Pitot Tubes and Probes Although the pitot tube is one of the simplest flow sensors, it is used in a wide range of flow measurement applications such as air speed in racing cars and Air Force fighter jets
Tagged as:Technical Learning, Get Curious
Read More![Specialty Level Switches](https://assets.omega.com/resources/t9904-15-spec-uf.jpg)
Specialty Level Switches Thermal, vibrating, and optical level switches are specialty devices developed to solve specific level detection problems.
Tagged as:Technical Learning, Get Curious
Read More![Electronic Flow meters](https://assets.omega.com/resources/electronic-flow-meter-uf.jpg)
Electronic Flow meters While the flow measurement technologies discussed in this chapter--magnetic, vortex, and ultrasonic--are neither exclusively nor exhaustively electronic in nature, they do represent a logical grouping of flow measurement technologies.
Tagged as:Technical Learning, Get Inspired
Read More![Monitoring Juice Level in a Vessel using Transmitters and Transducers](https://assets.omega.com/resources/flow-level-transmitters-pressure-monitoring-vessel-uf.jpg)
Monitoring Juice Level in a Vessel using Transmitters and Transducers The Role of Flow and Level Transmitters and Pressure Transducers in the Monitoring of Juice Level in a Vessel
Tagged as:Case Study, Get Going
Read More![Applying Ultrasonic Level Sensors in Cooling Tower Water Basins](https://assets.omega.com/resources/ultrasonic-level-transmitters-in-cooling-tower-water-basins-uf.jpg)
Applying Ultrasonic Level Sensors in Cooling Tower Water Basins Cooling towers are heat exchange systems that require precision sensors to ensure water basin liquid levels are monitored.
Tagged as:Technical Learning, Get Going
Read More![Ultrasonic Level Sensor Application in Above Ground Bulk Storage Tanks](https://assets.omega.com/resources/ultrasonic-level-transmitters-in-above-ground-bulk-storage-uf.jpg)
Ultrasonic Level Sensor Application in Above Ground Bulk Storage Tanks By installing level sensors, operators can be proactive and monitor liquid levels - ensuring environmental regulations associated with the design and operation are consistently met.
Tagged as:Technical Learning, Get Curious
Read More![Hybrid Ultrasonic Flow Meter Application Helps Ensure Accurate Enzyme Injection](https://assets.omega.com/resources/ultrasonic-flow-meters-enzyme-injection-monitoring-for-groundwater-remediation-oil-company-uf.jpg)
Hybrid Ultrasonic Flow Meter Application Helps Ensure Accurate Enzyme Injection Learn how flow meters helped an Oil company achieve accurate measurements of the water flow rate and total flow.
Tagged as:Case Study, Get Going
Read More![Flow Measurement in a Return Activated Sludge Line](https://assets.omega.com/resources/ultrasonic-flow-meter-return-activated-sludge-wwtp-uf.jpg)
Flow Measurement in a Return Activated Sludge Line Keene Waste Water Treatment Plant uses a secondary treatment process called activated sludge, a process which converts non-settable substances into a biological floc
Tagged as:Technical Learning, Get Going
Read More![The importance of wind tunnel testing in the lab](https://assets.omega.com/resources/importance-of-wind-tunnel-testing-in-the-lab-uf.jpg)
The importance of wind tunnel testing in the lab Failure rates for many electronic components rise with temperature.
Tagged as:Technical Learning, Get Curious
Read More![Doppler Meters Vs Transit Time Ultrasonic Flow Meters](https://assets.omega.com/resources/dif-between-doppler-transit-time-ultrasonic-flow-meters-uf.jpg)
Doppler Meters Vs Transit Time Ultrasonic Flow Meters Ultrasonic flow meters are non-intrusive devices that use acoustic vibrations to measure the flow rate of liquid...
Tagged as:Technical Learning, Get Curious
Read More![What is a Thermal Mass Flow Meter?](https://assets.omega.com/resources/thermal-mass-flow-working-principle-theory-and-design-uf.jpg)
What is a Thermal Mass Flow Meter? Thermal mass flow meters measure the mass flowrate of gases and liquids directly.
Tagged as:Technical Learning, Get Curious
Read More![Lessons about Positive Displacement Flow Meters](https://assets.omega.com/resources/positive-displacement-flow-meter-uf.jpg)
Lessons about Positive Displacement Flow Meters Positive Displacement flow meters are the only flow measuring technology to directly measure the volume of fluid that passes though the flow meter.
Tagged as:Technical Learning, Get Curious
Read More![Air Flow Measurement Instruments: How Precise and Accurate?](https://assets.omega.com/resources/how-precise-and-accurate-are-air-flow-measurement-instruments-uf.jpg)
Air Flow Measurement Instruments: How Precise and Accurate? Calculating flow rates through ducts, pipes, hoods and stacks (collectively called ducts for our purposes), has never been difficult.
Tagged as:Technical Learning, Get Curious
Read More![What is an Ultrasonic Flow Meter?](https://assets.omega.com/resources/ultrasonic-flow-meter-uf.jpg)
What is an Ultrasonic Flow Meter? An ultrasonic flow meter (non-intrusive Doppler flow meter) is a volumetric flow meter which requires particulates or bubbles in the flow.
Tagged as:Product Info, Get Curious
Read More![Anemometer](https://assets.omega.com/resources/anemometers-uf.jpg)
Anemometer An anemometer is an instrument used to measure the speed or velocity of gases either in a contained flow, such as airflow in a duct, or in unconfined flows, such as atmospheric wind.
Tagged as:Product Info, Get Curious
Read More![Level Measurement](https://assets.omega.com/resources/level-measurement-uf.jpg)
Level Measurement Integral to process control in many industries, level measurement sensors fall into two main types. Point level measurement sensors are used to mark a single discrete liquid height–a preset level condition.
Tagged as:Product Info, Get Curious
Read More![What are Electromagnetic Flow Meters?](https://assets.omega.com/resources/magmeter-uf.jpg)
What are Electromagnetic Flow Meters? A magnetic flow meter (mag flow meter) is a volumetric flow meter which does not have any moving parts and is ideal for wastewater applications or any dirty liquid which is conductive or water based.
Tagged as:Product Info, Get Curious
Read More