Skip to search Skip to main content Skip to navigation

Your feedback matters, take a quick surveyWebsite feedback

We noticed you are from . Visit your local site for regional offers and live support.
Technical Learning How to use Load Cells for Weight Measurement

How to use Load Cells for Weight Measurement To measure the weight, the subject is placed on a load application point of a load cell.

Read More
Technical Learning Load Cell Specifications

Load Cell Specifications In this article all the specifications in a load cell's datasheet are explained. Click here to learn and understand more about the technical aspects.

Read More
Technical Learning How to Test a Load Cell?

How to Test a Load Cell? Set the multimeter in millivolts and connect the output wires of the load cell to it. Supply a excitation voltage and place a test weight on the load cell.

Read More
Technical Learning Why Load Cell Signal Conditioner is Critical to a Strain Gauge Setup

Why Load Cell Signal Conditioner is Critical to a Strain Gauge Setup Signal conditioners take the output from the load cell, modify it and then send it to digital monitors or data loggers.

Read More
Technical Learning How to Pick a Data Logger for Your Load Cell?

How to Pick a Data Logger for Your Load Cell? A force to a load cell causes deformation on the strain gauge creating a electrical signal. A data logger takes that data and stores the data for later.

Read More
Technical Learning Load Cell Meter: Choosing the Right Strain Meters

Load Cell Meter: Choosing the Right Strain Meters The load cell meter connects directly to the strain gauge to convert the signal into a displayed value. They can also power up the load cell.

Read More
Technical Learning Load Cell FAQ

Load Cell FAQ Have questions about load cells?

Read More
Technical Learning Load Cell with Remote Display

Load Cell with Remote Display To accurately read and process the load cell values, displays form an essential part of the weighing system.

Read More
Technical Learning Load Cell Controller

Load Cell Controller A load cell controller is a device used in conjunction with a load cell to convert the electrical signals from the load cell to readable real-world values.

Read More
Technical Learning Load Cell Platform Scale – Example Illustration

Load Cell Platform Scale – Example Illustration For high-precision weighing applications, load cell platform scales must measure the load accurately. To illustrate this measurement precision, an example with a test weight is explained here.

Read More
Technical Learning What is a Load Cell Amplifier?

What is a Load Cell Amplifier? A load cell amplifier is a device that can increase the strength of signals coming from a load cell.

Read More
Technical Learning USB Load Cells: Do More with the Measurement Data

USB Load Cells: Do More with the Measurement Data Analog load cells can't record the data for further analysis. To make the load cell signals readable by a computer an USB output is useful. Read it here.

Read More
Application

How to Dynamically Measure Load and Vibration in Final Product Testing for Bicycle Manufacturing As part of a quality assurance process, a bike manufacturer developed a testing system that could quantify load and vibration forces on the physical parameters.

Read More
Technical Learning Using Load Cells to Weigh Trucks, Trains, and Aircraft

Using Load Cells to Weigh Trucks, Trains, and Aircraft In the airline industry, weight is money. Every additional pound requires more fuel to lift, so making sure there’s enough gas in the tanks means knowing what the aircraft weighs.

Read More
en-US
en
Save Configuration