When it comes to process piping systems, temperature of in-pipe media is often a necessary measurement – and one that needs to be monitored accurately. Traditionally, in-pipe immersion sensors are used. While immersion sensors are highly accurate and responsive to temperature change, they are also highly invasive, coming in direct contact with the process media in the pipe; not to mention the added maintenance cost and downtime associated with lengthy installation if a sensing location needs to be added or moved. As a result, invasive in-pipe immersion sensors are often not ideal for use within process piping systems.
Your feedback matters, take a quick surveyWebsite feedback