One of the most common questions asked is the difference between single-ended and differential signals inputs, and what applications they should be considered in.
Differential Signals
A signal input circuit where SIGNAL LO and SIGNAL HI are electrically floating with respect to ANALOG GROUND. For example, a differential input A/D card will have one HI (+) and one LOW (-) pin for each input.
There will also be a LLGND (LOW LEVEL GROUND) pin which may be used if a ground connection is required. This allows the measurement of the voltage difference between two signals tied to the same ground and provides superior common-mode noise rejection.
Where should differential signal inputs be used?
Whenever electromagnetic interference (EMI) or radio frequency interference (RFI) is present, a voltage can be induced on BOTH signal wires.
A differential input amplifier will reject the COMMON MODE VOLTAGE, provided that the common mode voltage plus the input signal does not exceed the device's CMR specification. The effect on a single-ended input is usually a voltage fluctuation between signal high and signal ground.
Single-ended inputs
A single signals input has no commond mode range because there is only ONE low wire, which is shared by all inputs.
For example, if you have an A/D board with 16 single-ended inputs, there will be 16 HIGH (+) lines and one LOW (-) line (sometimes called LLGND). Some cards may have several LOW lines to provide extra places to make your ground connection, however, these lines are tied together and are basically the same thing.
When to use single-ended or Differential signals?
Differential inputs provide a more stable reading when EMI or RFI is present, and therefore, it is recommended to use them whenever noise is generally a problem. This is especially true when measuring thermocouple, strain gage and bridge type pressure sensor inputs, since they produce very small signals that are very succeptible to noise. Single-ended inputs are lower in cost, and provide twice the number of inputs for the same size wiring connector, since they require only one analog HIGH (+) input per channel and one LLGND (-) shared by all inputs. Differential signals require signal HIGH and LOW inputs for each channel and one common shared LLGND. Single-ended inputs save connector space, cost, and are easier to install.