Skip to search Skip to main content Skip to navigation

PST joins DwyerOmega. Read more>

We noticed you are from . Visit your local site for regional offers and live support.
Case Study Improved Diagnostic Information Resulted in Significant Cost Savings

Improved Diagnostic Information Resulted in Significant Cost Savings On a recent project the data used provided by DRST-CM to develop software modules in the DCS that provide full diagnostics, a client’s company has been able to use the data for preventive maintenance.

Read More
Case Study Unique Solutions to Challenging Automation Applications

Unique Solutions to Challenging Automation Applications In pursuit of weight savings, aerospace companies are moving towards more exotic materials. While stronger and lighter, these materials are also...

Read More
Technical Learning 5 Ways the Right Expertise Can Simplify the Customization Process

5 Ways the Right Expertise Can Simplify the Customization Process Pressure transducers and load cells play a critical role in ensuring the safety, reliability, and accuracy of products and processes across a wide variety of industries—including aerospace, mining, manufacturing, technology, and more.

Read More
Case Study Hybrid Ultrasonic Flow Meter Application Helps Ensure Accurate Enzyme Injection

Hybrid Ultrasonic Flow Meter Application Helps Ensure Accurate Enzyme Injection Learn how flow meters helped an Oil company achieve accurate measurements of the water flow rate and total flow.

Read More
Technical Learning Flow Measurement in a Return Activated Sludge Line

Flow Measurement in a Return Activated Sludge Line Keene Waste Water Treatment Plant uses a secondary treatment process called activated sludge, a process which converts non-settable substances into a biological floc

Read More
Technical Learning What is MI Cable?

What is MI Cable? The basic construction provides high-temperature capability, exceptional electrical isolation, and physical protection for the conductors especially when subjected to harsh environments.

Read More
Technical Learning High Temperature Pressure Transducers vs. Cooling Elements

High Temperature Pressure Transducers vs. Cooling Elements Pressure measurement is often a challenging task due to the harsh environments frequently found in industrial manufacturing.

Read More
Technical Learning Types of Relays

Types of Relays Relays are the control switches that operate with low-powered electrical signals controlling most types of circuits.

Read More
Product Info M12 Temperature Sensors

M12 Temperature Sensors Temperature sensors provide an input to a system (indicator, controller or other device) that is used to determine the temperature of a specific process or location.

Read More
Technical Learning Installing a Load Cell: Best Practices

Installing a Load Cell: Best Practices Each load cell installation is unique. Consult a structural engineer when your application requires very high accuracy, long-term stability, custom specifications, or when using in a varied R&D environment.

Read More
Technical Learning Understanding Deadband for Pressure Switches

Understanding Deadband for Pressure Switches A pressure switch consists of a sensing component and an electrical switch.

Read More
Product Info Reversible & Non Reversible Temperature Labels & Sensors

Reversible & Non Reversible Temperature Labels & Sensors Temperature labels are temperature monitors consisting of one or more small heat-sensitive indicators sealed under transparent, heat-resistant windows.

Read More
Product Info Stepper Motors

Stepper Motors A stepper motor is a brushless, synchronous electric motor that converts digital pulses into mechanical shaft rotation.

Read More
Product Info What is a Pressure Gauge?

What is a Pressure Gauge? Pressure gauges are among the most often used instruments in a plant. But because of their great numbers, attention to maintenance--and reliability--can be compromised.

Read More
en-US
en
Save Configuration