Skip to search Skip to main content Skip to navigation

Your feedback matters, take a quick surveyWebsite feedback

We noticed you are from . Visit your local site for regional offers and live support.
Product Info What is a Thermal Imaging Camera?

What is a Thermal Imaging Camera? A thermal imager is a non-contact temperature measurement device.

Read More
Product Info Remote monitoring for challenging times

Remote monitoring for challenging times How can remote monitoring help your application stay afloat and keep employees safe

Read More
Product Info An Introduction to Flow Meters

An Introduction to Flow Meters As the name implies a Flow meter is an instrument for monitoring, measuring, or recording the rate of flow, pressure, or discharge of liquids or gasses.

Read More
Product Info Thermocouple styles: probe, wire or surface?

Thermocouple styles: probe, wire or surface? Because a thermocouple can take many shapes and forms, it is important to understand how to correctly select the right sensor.

Read More
Product Info What is a PID Controller?

What is a PID Controller? A PID controller is an instrument used in industrial control applications to regulate temperature, flow, pressure, speed and other process variables.

Read More
Product Info How to choose a Thermocouple

How to choose a Thermocouple There are different types of thermocouples and their applications may vary. An exposed thermocouple will work best when high response times are required, but an ungrounded thermocouple is better in corrosive environments

Read More
Product Info How to Choose Between a RTD PT100 vs Pt1000?

How to Choose Between a RTD PT100 vs Pt1000? The sensing elements in Resistance Temperature Detectors (RTD’s) can be categorized in terms of the type of metal out of which they’re made and their resistance at a benchmark temperature.

Read More
Product Info Types of RTDs

Types of RTDs Resistance Temperature Detectors (RTDs) available today can generally be categorized into one of two basic types of RTDs, depending on how their temperature sensing element is constructed.

Read More
Product Info What Are the Differences Between 2-Wire, 3-Wire, and 4-Wire RTD Configurations?

What Are the Differences Between 2-Wire, 3-Wire, and 4-Wire RTD Configurations? A Resistance Temperature Detector (RTD) measures temperature using a resistor with a resistance value that changes as its temperature increases or decreases.

Read More
Product Info Temperature Control Using PID

Temperature Control Using PID Almost every process control application would benefit from PID control.

Read More
Product Info How Does a PID Controller Work?

How Does a PID Controller Work? As its name implies, a PID controller combines proportional control with additional integral and derivative adjustments which help the unit automatically compensate for changes in the system.

Read More
Product Info Working principle of thermocouples

Working principle of thermocouples A typicial thermocouple is made up of two dissimilar metals joined together to form two junctions.

Read More
Product Info Sanitary Sensors

Sanitary Sensors A Sanitary Sensor is a device which measures temperature, flow or pressure in an environment where products will be for human consumption.

Read More
Product Info M12 Temperature Sensors

M12 Temperature Sensors Temperature sensors provide an input to a system (indicator, controller or other device) that is used to determine the temperature of a specific process or location.

Read More
Product Info Grippers

Grippers A gripper is a motion device that mimics the movements of people, in the case of the gripper, it is the fingers.

Read More
Product Info OEM

OEM Our commitment to maintaining the leading edge through research development and state-of-the art manufacturing keeps OMEGA firmly at the forefront of technology.

Read More
Product Info Strip Heater

Strip Heater A strip heater is a device which is mounted on a surface and used to heat the surface or air (gasses).

Read More
Product Info Calibrator

Calibrator A calibrator is an equipment used to adjust an instrument accuracy, often associated with a specific application.

Read More
Product Info Cryogenic Temperature Sensors

Cryogenic Temperature Sensors Cryogenics is the branch of physics that deals with the production and effects of very low temperatures.

Read More
Product Info Temperature Measurement

Temperature Measurement Temperature can be measured via a diverse array of sensors. All of them infer temperature by sensing some change in a physical characteristic.

Read More
Product Info Wireless Sensors

Wireless Sensors Wireless sensors are standard measurement tools equipped with transmitters to convert signals from process control instruments into a radio transmission.

Read More
Product Info Remote Monitoring

Remote Monitoring Ethernet/internet-based data monitoring brings new capabilities and unprecedented access to process measurement and control.

Read More
Product Info IC Sensors

IC Sensors An IC Temperature Sensor is a two terminal integrated circuit temperature transducer that produces an output current proportional to absolute temperature. The sensor package is small with a low thermal mass and a fast response time

Read More
Product Info Data Acquisition

Data Acquisition In the simplest form, a technician logging the temperature of an oven on a piece of paper is performing data acquisition.

Read More
Product Info Panel Meters

Panel Meters A panel meter is an instrument that displays an input signal in either a digital or analog form.

Read More
Product Info Reversible & Non Reversible Temperature Labels & Sensors

Reversible & Non Reversible Temperature Labels & Sensors Temperature labels are temperature monitors consisting of one or more small heat-sensitive indicators sealed under transparent, heat-resistant windows.

Read More
Product Info Infrared Thermometer

Infrared Thermometer On its most basic design an infrared thermometer consists of a lens to focus the infrared (IR) energy on to a detector.

Read More
Product Info Chart Recorders

Chart Recorders A chart recorder is an instrument used to record various process and electrical signals.

Read More
Product Info What is a Temperature Controller?

What is a Temperature Controller? As the name implies, a temperature controller is an instrument used to control temperatures, mainly without extensive operator involvement.

Read More
Product Info What Is A Pressure Transducer?

What Is A Pressure Transducer? A pressure transducer, often called a pressure transmitter, is a transducer that converts pressure into an analog electrical signal. Although there are various types of pressure transducers, one of the most common is the strain-gage base transducer.

Read More
Product Info What is an Ultrasonic Flow Meter?

What is an Ultrasonic Flow Meter? An ultrasonic flow meter (non-intrusive Doppler flow meter) is a volumetric flow meter which requires particulates or bubbles in the flow.

Read More
Product Info What Is A Thermistor And How Does It Work?

What Is A Thermistor And How Does It Work? A thermistor is an element with an electrical resistance that changes in response to temperature.

Read More
Product Info Anemometer

Anemometer An anemometer is an instrument used to measure the speed or velocity of gases either in a contained flow, such as airflow in a duct, or in unconfined flows, such as atmospheric wind.

Read More
Product Info Stepper Motors

Stepper Motors A stepper motor is a brushless, synchronous electric motor that converts digital pulses into mechanical shaft rotation.

Read More
Product Info Strain Gauges

Strain Gauges A Strain gage (sometimes referred to as a Strain Gauge) is a sensor whose resistance varies with applied force; It converts force, pressure, tension, weight, etc., into a change in electrical resistance which can then be measured.

Read More
Product Info How to Measure Acceleration?

How to Measure Acceleration? An accelerometer is a device that measures the vibration, or acceleration of motion of a structure.

Read More
Product Info What is a Flexible Heater?

What is a Flexible Heater? A flexible heater is a device which can conform to the surface which requires heating.

Read More
Product Info Data Loggers

Data Loggers Technically speaking, a data logger is any device that can be used to store data.

Read More
Product Info Industrial Heaters

Industrial Heaters Electric heaters are used in a variety of processes where the temperature of an object or process needs to be increased.

Read More
Product Info Level Measurement

Level Measurement Integral to process control in many industries, level measurement sensors fall into two main types. Point level measurement sensors are used to mark a single discrete liquid height–a preset level condition.

Read More
Product Info Thermocouple Wire

Thermocouple Wire Wire that is used in a thermocouple from the point of sensing to the point of cold junction compensation (cjc end) where the signal is measured.

Read More
Product Info What are Electromagnetic Flow Meters?

What are Electromagnetic Flow Meters? A magnetic flow meter (mag flow meter) is a volumetric flow meter which does not have any moving parts and is ideal for wastewater applications or any dirty liquid which is conductive or water based.

Read More
Product Info Immersion Heater

Immersion Heater An immersion heater is a device which is installed in a tank or container to heat a liquid. The installation can be over-the-side, flanged or threaded.

Read More
Product Info What is a Pressure Gauge?

What is a Pressure Gauge? Pressure gauges are among the most often used instruments in a plant. But because of their great numbers, attention to maintenance--and reliability--can be compromised.

Read More
en-US
en
Save Configuration