![Flow Meter Tutorial](https://assets.omega.com/resources/flow-meter-tutorial-uf.jpg)
Flow Meter Tutorial So you want to measure flow? The answer would seem to be to purchase a flowmeter.
Tagged as:Technical Learning, Get Curious
Read More![What is a Low Pass Filter?](https://assets.omega.com/resources/data-acquisition-reduce-signal-low-pass-filters-uf.jpg)
What is a Low Pass Filter? A low pass filter is placed on the signal wires between a signal and an A/D board
Tagged as:Technical Learning, Get Curious
Read More![Technical Principles of Valves](https://assets.omega.com/resources/valves-technical-principles-uf.jpg)
Technical Principles of Valves Solenoid valves are used wherever fluid flow has to be controlled automatically. They are being used to an increasing degree in the most varied types of plants and equipment.
Tagged as:Technical Learning, Get Curious
Read More![An Introduction to Venturi Flow Meters, Flow Nozzles, and Segmental Wedge Elements](https://assets.omega.com/resources/venturi-meter-uf.jpg)
An Introduction to Venturi Flow Meters, Flow Nozzles, and Segmental Wedge Elements Venturi tubes are available in sizes up to 7 inches and can pass 25 to 50% more flow than an orifice with the same pressure drop
Tagged as:Technical Learning, Get Curious
Read More![What is an Orifice Plate Flow Meter?](https://assets.omega.com/resources/orifice-plate-flow-meter-uf.jpg)
What is an Orifice Plate Flow Meter? The orifice plate flow meter is commonly used in clean liquid, gas, and steam services. It is available for all pipe sizes but it is very cost-effective for measuring flows in larger ones (over 6 inches diameter).
Tagged as:Technical Learning, Get Curious
Read More![RS485, RS422 and RS232](https://assets.omega.com/resources/rs422-rs485-rs232-uf.jpg)
RS485, RS422 and RS232 Why use RS232 vs RS485 and what is the real difference between RS422 Vs RS485? First, lets define each one. Keep in mind that all three are considered SERIAL, as opposed to IEEE-488 which is PARALLEL.
Tagged as:Technical Learning, Get Curious
Read More![Monitoring Juice Level in a Vessel using Transmitters and Transducers](https://assets.omega.com/resources/flow-level-transmitters-pressure-monitoring-vessel-uf.jpg)
Monitoring Juice Level in a Vessel using Transmitters and Transducers The Role of Flow and Level Transmitters and Pressure Transducers in the Monitoring of Juice Level in a Vessel
Tagged as:Case Study, Get Going
Read More![Science Team Sets Out to Measure Just How Strong a Python Is, Using a Pressure Transducer](https://assets.omega.com/resources/just-how-strong-is-a-python-uf.jpg)
Science Team Sets Out to Measure Just How Strong a Python Is, Using a Pressure Transducer Our engineers help design a system that will figure out just how much deadly force a python really has.
Tagged as:Case Study, Get Inspired
Read More![Ultrasonic Level Sensor Application in Above Ground Bulk Storage Tanks](https://assets.omega.com/resources/ultrasonic-level-transmitters-in-above-ground-bulk-storage-uf.jpg)
Ultrasonic Level Sensor Application in Above Ground Bulk Storage Tanks By installing level sensors, operators can be proactive and monitor liquid levels - ensuring environmental regulations associated with the design and operation are consistently met.
Tagged as:Technical Learning, Get Curious
Read More![Using Load Cells to Weigh Trucks, Trains, and Aircraft](https://assets.omega.com/resources/using-load-cells-to-weigh-trucks-trains-aircraft-uf.jpg)
Using Load Cells to Weigh Trucks, Trains, and Aircraft In the airline industry, weight is money. Every additional pound requires more fuel to lift, so making sure there’s enough gas in the tanks means knowing what the aircraft weighs.
Tagged as:Technical Learning, Get Going
Read More