![](https://assets.omega.com/resources/ultrasonic-flow-meter-water-leak-us.png)
How to Locate a Water Leak Using an Ultrasonic Flow Meter When a single conduit line in a complex configuration of pipelines is compromised, it can be challenging to locate the precise point where the leak is occurring.
Tagged as:Application, Get Curious
Read More![](https://assets.omega.com/resources/temperature-measurement-coffee-grinder-us.jpg)
How to Measure an Industrial Coffee Grinder Motor’s Temperature During Grinding In this application, the purpose is to measure the temperature of the motor in an industrial coffee grinder during the grinding process to better understand the strain on the motor.
Tagged as:Application, Get Curious
Read More![](https://assets.omega.com/resources/temperature-measurement-appliances-us.png)
How to Wirelessly Monitor Temperature for Performance Testing As part of the quality assurance process on refrigeration equipment such as refrigerators, freezers, and cold rails, there is a need to validate that the equipment is operating within specified parameters.
Tagged as:Application, Get Curious
Read More![](https://assets.omega.com/resources/temperature-control-mantle-heater-us.png)
Benchtop Controller for Mantle Heater Heating mantles are commonly used in laboratories to heat liquids as part of the research process.
Tagged as:Application, Get Curious
Read More![](https://assets.omega.com/resources/pid-control-heating-system-us.jpg)
How to Achieve Precise Temperature Regulation of Experimental Materials Using a PID-Controlled Heat Source in Laboratory Applications To investigate whether the thermochromic phase change behavior of polydiacetylene thin films will be altered when placed onto a carbon substrate such as graphene, a researcher developed a transfer heat block whose temperature could be regulated over time.
Tagged as:Application, Get Curious
Read More![](https://assets.omega.com/resources/ph-measurement-high-temperature-us.png)
How to Monitor pH Levels in a High-Temperature Environment In a process application, such as soaking wood in a water bath, unpleasant odors can be omitted. By neutralizing pH levels in the water bath, odors can be controlled.
Tagged as:Application, Get Curious
Read More![](https://assets.omega.com/resources/ph-measurement-digestive-system-us.jpg)
How to Measure pH Levels in a Ruminant’s Digestive System The pH levels in each of a ruminant’s four stomachs play an essential role in a cow’s digestive process and milk production.
Tagged as:Application, Get Curious
Read More![](https://assets.omega.com/resources/load-vibration-measurement-bicycles-us.png)
How to Dynamically Measure Load and Vibration in Final Product Testing for Bicycle Manufacturing As part of a quality assurance process, a bike manufacturer developed a testing system that could quantify load and vibration forces on the physical parameters.
Tagged as:Application, Get Curious
Read More![](https://assets.omega.com/resources/load-measurement-cables-us.jpg)
How to Test Load Tolerance in Control Cable Product Testing Control cables play a critical role in assuring the safety and operational integrity of a wide variety of mechanical and electromechanical devices, including lawn mowers and bicycles.
Tagged as:Application, Get Curious
Read More![](https://assets.omega.com/resources/force-measurement-rocket-us.jpg)
Measuring the Force Applied to a Rocket Parachute Rockets deploy parachutes to aid in rapidly decreasing the rocket’s re-entry or landing speed. However, before use, it’s essential to test the system using s-beam load cells.
Tagged as:Application, Get Curious
Read More![](https://assets.omega.com/resources/force-measurement-metal-bending-us.jpg)
How to Measure the Bending Force of a Sheet Metal Bending Machine Measuring bending stress requires determining the average amount of force exerted on the material that results in a repeatable uniform surface.
Tagged as:Application, Get Curious
Read More![](https://assets.omega.com/resources/force-measurement-crossbow-us.jpg)
How to Determine the Force Measurement of a Crossbow Crossbows work like a spring. The force and tension applied as you pull the string of the crossbow is what creates the movement and energy to propel the arrow from the bow at high speed.
Tagged as:Application, Get Curious
Read More![](https://assets.omega.com/resources/flow-meter-paper-stock-us.jpg)
Flow of Paper Stock A customer in the paper industry wanted to measure flow of paper stock pulp on a 250mm SS line with an average flow of 120-150 l/s and a pulp temperature of 45°.
Tagged as:Application, Get Curious
Read More![](https://assets.omega.com/resources/flow-measurement-microbreweries-uf.jpg)
Sanitary Precision Flow Measurement for Microbreweries All microbreweries need the ability to measure the liquid flow of their product in a manner that is sanitary and meets FDA regulations.
Tagged as:Application, Get Curious
Read More![](https://assets.omega.com/resources/flexible-heater-bending-guitar-uf.jpg)
How to Bend Guitar Sides with a Silicone Heater There are several ways to bend guitar sides, including the traditional method of using a hot pipe. However, a faster and more cost-efficient method, which has become common, involves using flexible silicone heaters with a flexible thermocouple and controller.
Tagged as:Application, Get Curious
Read More![](https://assets.omega.com/resources/pizza-image-uf.png)
How to Maintain the Perfect Temperature in a Pizza Oven If you want your pizzas to come out cooked to perfection every time, you need to make sure that your oven temperature consistently maintains the right temperature.
Tagged as:Application, Get Inspired
Read More