![temperature](https://assets.omega.com/resources/iStock-1311412442@3x.png)
When it comes to industrial processing applications, temperature measurement is often of utmost importance – and is so for a myriad of reasons. It serves, for example, as a fundamental control parameter, influencing the quality and consistency of manufactured products, process efficiency, and, most importantly, safety. Monitored accurately, it ensures that materials are processed within specified temperature ranges, preventing defects and ensuring product integrity.
Temperature can be measured via a diverse array of sensors, and all of them infer temperature by sensing some change in a physical characteristic. The six types with which an engineer is most likely to come into contact are:
- Thermocouples
- Resistance Temperature Devices
- Infrared Radiators
- Bimetallic Devices
- Liquid Expansion Devices
- Change-of-State Devices
The Workhorses
In the chemical process industries, the most commonly used temperature sensors are thermocouples, resistive devices, and infrared devices. There is widespread misunderstanding as to how these devices work and how they should be used.
Thermocouples
Consider first the thermocouple – probably the most-often-used and least-understood of the three. Essentially, a thermocouple consists of two alloys joined together at one end and open at the other. The emf at the output end (the open end; V1 in Figure 1a) is a function of the temperature T1 at the closed end. As the temperature rises, the emf goes up.
Often, the thermocouple is located inside a metal or ceramic shield that protects it from a variety of environments. Metal-sheathed thermocouples are also available with many types of outer coatings, such as polytetrafluoroethylene, for trouble-free use in corrosive solutions.
![temperature](https://assets.omega.com/resources/Rectangle271@3x.png)
![temperature](https://assets.omega.com/resources/Group2712@3x.png)
![temperature](https://assets.omega.com/resources/Rectangle271@3x.png)
![temperature](https://assets.omega.com/resources/Group2723@3x.png)
The open-end emf is a function of not only the closed-end temperature (i.e., the temperature at the point of measurement), but also the temperature at the open end (T2 in Figure 1a). Only by holding T2 at standard temperature can the measured emf be considered a direct function of the charge in T1. The industrially accepted standard for T2 is 0 °C; therefore, most tables and charts make the assumption that T2 is at that level. In industrial instrumentation, the difference between the actual temperature at T2 and 0 °C is usually corrected for electronically, within the instrumentation. This emf adjustment is referred to as the cold-junction, or CJ, correction.
Temperature changes in the wiring between the input and output ends do not affect the output voltage, provided that the wiring is of thermocouple alloy or a thermoelectric equivalent (Figure 1a). For example, if a thermocouple is measuring temperature in a furnace and the instrument that shows the reading is some distance away, the wiring between the two could pass near another furnace and not be affected by its temperature, unless it becomes hot enough to melt the wire or permanently change its electrothermal behavior.
![temperature](https://assets.omega.com/resources/Rectangle271@3x.png)
![temperature](https://assets.omega.com/resources/Group2734@3x.png)
![temperature](https://assets.omega.com/resources/Rectangle271@3x.png)
![temperature](https://assets.omega.com/resources/Group2743@3x.png)
The composition of the junction itself does not affect the thermocouple action in any way, so long as the temperature T1 is kept constant throughout the junction and the junction material is electrically conductive (Figure 1b). Similarly, the reading is not affected by insertion of non-thermocouple alloys in either or both leads, provided that the temperature at the ends of the “spurious” material is the same (Figure 1c).
This ability of the thermocouple to work with a spurious metal in the transmission path enables the use of a number of specialized devices, such as thermocouple switches. Whereas the transmission wiring itself is normally the thermoelectrical equivalent of the thermocouple alloy, properly operating thermocouple switches must be made of gold-plated or silver-plated copper allow elements with appropriate steel springs to ensure good contact. So long as the temperatures at the input and output junctions of the switch are equal, this change in composition makes no difference.
It is important to be aware of what might be called the Law of Successive Thermocouples. Of the two elements that are shown in the upper portion of Figure 1d, one thermocouple has T1 at the hot end and T2 at the open end. The second thermocouple has its hot end at T2 and its open end at T3. The emf level for the thermocouple that is measuring T1 is V1; that for the other thermocouple is V2. The sum of the two emfs, V1 plus V2, equals the emf V3 that would be generated by the combined thermocouple operating between T1 and T3. By virtue of this law, a thermocouple designated for one open-end reference temperature can be used with a different open-end temperature.
RTDs
A typical RTD consists of a fine platinum wire wrapped around a mandrel and covered with a protective coating. Usually, the mandrel and coating are glass or ceramic. The mean slope of the resistance vs. temperature plot for the RTD is often referred to as the alpha value (Figure 2), alpha standing for the temperature coefficient. The slope of the curve for a given sensor depends somewhat on the purity of the platinum in it.
![temperature](https://assets.omega.com/resources/Group2748@3x.png)
![temperature](https://assets.omega.com/resources/tempChartText@3x.png)
The most commonly used standard slope, pertaining to platinum of a particular purity and composition. Has a value of 0.00385 (assuming that the resistance is measured in ohms and the temperature in degrees Celsius). A resistance vs. temperature curve drawn with this slope is a so-called European curve, because RTDs of this composition were first used extensively on that continent. Complicating the picture, there is also another standard slope, pertaining to a slightly different platinum composition. Having a slightly higher alpha value of 0.00392, it follows what is known as the American curve.
If the alpha value for a given RTD is not specified, it is usually 0.00385. However, it is prudent to make sure of this, especially if the temperatures to be measured are high. This point is brought out in Figure 2, which shows both the European and American curves for the most widely used RTD, namely one that exhibits 100 ohms resistance at 0 °C.
Thermistors
The resistance-temperature relationship of a thermistor is negative and highly non-linear. This poses a serious problem for engineers who must design their own circuitry. However, the difficulty can be eased by using thermistors in matched pairs, in such a way that the nonlinearities offset each other. Furthermore, vendors offer panel meters and controllers that compensate internally for thermistors’ lack of linearity.
Thermistors are usually designated in accordance with their resistance at 25 °C. The most common of these ratings is 2252 ohms; among the others are 5,000 and 10,000 ohms. If not specified to the contrary, most instruments will accept the 2252 of thermistor.
Infrared Sensors
These measure the amount of radiation emitted by a surface. Electromagnetic energy radiates from all matter regardless of its temperature. In many process situations, the energy is in the infrared region. As the temperature goes up, the amount of infrared radiation and its average frequency go up.
Different materials radiate at different levels of efficiency. This efficiency is quantified as emissivity, a decimal number or percentage ranging between 0 and 1 or 0% and 100%. Most organic materials, including skin, are very efficient, frequently exhibiting emissivities of 0.95. Most polished metals, on the other hand, tend to be inefficient radiators at room temperature, with emissivity or efficiency often 20% or less.
To function properly, an infrared measurement device must consider the emissivity of the surface being measured. This can often be looked up in a reference table. However, bear in mind that tables cannot account for localized conditions such as oxidation and surface roughness. A sometimes practical way to measures temperature with infrared when the emissivity level is not known is to “force” the emissivity to a known level, by covering the surface with masking tape (emissivity of 95%) or a highly emissive paint.
Some of the sensor input may well consist of energy that is not emitted by the equipment or material whose surface is being targeted, but instead is being reflected by that surface from other equipment or materials. Emissivity pertains to energy radiating from a surface, whereas “reflection” pertains to energy reflected from another source. Emissivity of an opaque material is an inverse indicator of its reflectivity – substances that are good emitters do not reflect much incident energy, and thus do not pose much of a problem to the sensor in determining surface temperatures. Conversely, when one measures a target surface with only, say, 20% emissivity, much of the energy reaching from something like a nearby furnace at some other temperature. In short, be wary of hot, spurious reflected targets.
An infrared device is like a camera, and thus covers a certain field of view. It might, for instance, be able to “see” to a 1-degree visual cone or a 100-degree cone. When measuring a surface, be sure that the surface completely fills the field of view. If the target surface does not at first fill the field of view, move closer, or use an instrument with a narrower field of view. Or, simply take the background temperature into account when reading the instrument.
Selection Guides
RTDs are more stable than thermocouples. On the other hand, as a class, their temperature range is not as broad: RTDs operate from about -250 to 850 °C (-418 to 1562 °F), whereas thermocouples range from about -270 to 2300 °C (-457 to 4172 °F). Thermistors have a more restrictive span, being commonly used between -40 and 150 °C (-40 and 302 °F), but offer high accuracy in that range.
Thermistors and RTDs share a very important limitation: they are resistive devices, and, accordingly, they function by passing a current through a sensor. Even though only a very small current is generally employed, it creates a certain amount of heat and thus can throw off the temperature reading. This self-heating in resistive sensors can be significant when dealing with a still fluid because there is less carry-off of the heat generated. This problem does not arise with thermocouples, which are essentially zero-current devices.
Infrared sensors, though relatively expensive, are appropriate when the temperatures are extremely high. They are available for up to 3000 °C (5400 °F), far exceeding the range of thermocouples or other contact devices.
The infrared approach is also attractive when one does not wish to make contact with the surface whose temperature is to be measured. Thus, fragile or wet surfaces, such as painted surfaces coming out of a drying oven, can be monitored in this way. Substances that are chemically reactive or electrically noisy are ideal candidates for infrared measurement. The approach is likewise advantageous in measuring temperature of very large surfaces – such as walls – that would require a large array of thermocouples or RTDs for measurement.
To learn more about Omega Engineering’s selection of high-quality, expertly engineered, American-made Temperature Measurement products, please click here.