For added convenience and versaility OMEGA offers these Temperature Test Kits. The OMEGAMARKER crayon is easy to use, but certain conditions must be considered. OMEGAMARKERS will not make any mark on smooth or rough surfaces in cold conditions. When rubbed hard on a rough surface, the OMEGAMARKER gets ground and the powder is deposited on the surface which appears like a mark, but will not adhere. The correct way of using OMEGAMARKERS would be to strike it across a pre-heated surface during the heating process, using proper safety precautions. While the temperature is below the rated temperature there will not be a visible mark, but as soon as the surface reaches the rated temperature of the marker, at the point of contact the marker will melt and make a visible mark on the surface. This is an indication that the surface has reached the rated temperature of the OMEGAMARKER.
Each of the four kits contains 10 crayons. Three kits have pre-selected values. The fourth, the custom kit, has values that can be selected by the user.
Full Range Kit
°F: 125 200 250 300 350 425 500 575 650 750
°C: 52 93 121 149 177 218 260 302 343 399
Low Range Kit
°F: 125 150 175 200 225 250 275 300 325 350
°C: 52 66 79 93 107 121 135 149 163 177
High Range Kit
°F: 300 350 400 450 500 550 600 650 700 750
°C: 149 177 204 232 260 288 316 343 371 399
Custom Kit, Select 10 Crayons from among:
Deg. F | Deg. C | ![](/images/t.gif) | Deg. F | Deg. C | ![](/images/t.gif) | Deg. F | Deg. C | ![](/images/t.gif) | Deg. F | Deg. C | ![](/images/t.gif) | Deg. F | Deg. C |
100 | 38 | 200 | 93 | 294 | 146 | 392 | 200 | 550 | 288 |
104 | 40 | 203 | 95 | 300 | 149 | 400 | 204 | 554 | 290 |
109 | 43 | 206 | 97 | 302 | 150 | 410 | 210 | 572 | 300 |
119 | 48 | 212 | 100 | 306 | 152 | 413 | 212 | 575 | 302 |
122 | 50 | 213 | 101 | 311 | 155 | 419 | 215 | 600 | 316 |
125 | 52 | 219 | 104 | 313 | 156 | 425 | 218 | 650 | 343 |
131 | 55 | 225 | 107 | 320 | 160 | 428 | 220 | 662 | 350 |
140 | 60 | 230 | 110 | 325 | 163 | 437 | 225 | 700 | 371 |
150 | 66 | 239 | 115 | 329 | 165 | 446 | 230 | | |
158 | 70 | 248 | 120 | 338 | 170 | 450 | 232 | | |
163 | 73 | 250 | 121 | 344 | 173 | 455 | 235 | | |
167 | 75 | 256 | 124 | 347 | 175 | 463 | 239 | | |
169 | 76 | 257 | 125 | 350 | 177 | 475 | 246 | | |
175 | 79 | 263 | 128 | 356 | 180 | 482 | 250 | | |
176 | 80 | 266 | 130 | 363 | 184 | 488 | 253 | | |
182 | 83 | 269 | 132 | 374 | 190 | 500 | 260 | | |
185 | 85 | 275 | 135 | 375 | 191 | 518 | 270 | | |
188 | 87 | 284 | 140 | 383 | 195 | 525 | 274 | | |
194 | 90 | 288 | 142 | 388 | 198 | 536 | 280 | | |